Part Number: LP-CC2652RB
Other Parts Discussed in Thread: Z-STACK
Hello! My Project is based on two main tasks: "sampleApp_task" (Application task entry point for the Z-Stack)
and "Mc2MainTask" : my task, declared and started in the same way as other task.
Both tasks are configured inside main() function:
-----------------------------------------------------------------------------------
/* Configure app task. */
Task_Params_init(&taskParams);
taskParams.stack = myTaskStack;
taskParams.stackSize = APP_TASK_STACK_SIZE;
taskParams.priority = 2;// Priorità maggiorex Stack ?
Task_construct(&myTask, taskFxn, &taskParams, NULL);
/// Add another task for application specific logic
Task_Params_init(&taskParams2);
taskParams2.stack = myTaskStack2;
taskParams2.stackSize = APP_TASK_STACK_SIZE;
taskParams2.priority = 2;
Task_construct(&myTask2, taskFxn2, &taskParams2, NULL);
-----------------------------------------------------------------------------------
Here is the question: at the beginning can I launch only my application, then after some time launch "sampleApp_task" (from my task?)
Likewise: can I restart "sampleApp_task" along my task ?
As you can see I'm not so familiar about handling tasks.... I hope someone can help me with few C source lines....
Thanks a lot
Luigi