Part Number: CC2652P
Other Parts Discussed in Thread: Z-STACK
When the device communicates with the gateway, the packet catcher will catch this data. What is the reason

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
SDK version :simplelink_cc13x2_26x2_sdk_5_10_00_48
I can't use default example and see this.The sdk runs on our hardware, which is not always the case.
Hi liu,
Given that this cannot be replicated on a default example, I recommend that you further investigate what is necessary to cause the behavior and which change to the stack is making the packets appear. I see some inconsistencies from the screenshot such as ZC Transport Key messages before a ZED Data Request (as though the end device associated as non-sleepy or with FFD capabilities) and a Beacon being sent from the ZED although this should not be enabled on a RFD. There are also MAC Sequence numbers missing for the ZED which represents packets not shown by the sniffer log. Please make sure that there is no confusion in the project as to the device's determined role.
Regards,
Ryan