Part Number: CC1352P7
Other Parts Discussed in Thread: SYSCONFIG
HI TI!!!
I am perzonalizing the sample project zr_sw_ota_client_onchip_LP_CC1352P7_4 SDK 7.10.
OTA works perfectly without customizing the board.
But I need to customize the board to configure internal differential bias.
So I build, copy and save the ti_driver_config.c/h files and then customize the board and enable internal differential bias.
With the above described customization OTA does not work correctly. After doing OTA the first time I try to do OTA a second time and it gets stuck at 10%. If I reboot it runs the image loaded by JTAG.
(Of course I take into account the momoria slots).
Without customizing the board everything works perfectly.
How can I solve it?
How can I enable internal differential bias without customizing the board?
Thanks!