Part Number: CC2538EMK
Other Parts Discussed in Thread: CC2538, SMARTRF06EBK, SMARTRFTM-STUDIO
Hello,
I have a CC2538 development kit, when I try to use it in windows laptop using the USB cable that came with the kit. The SmartRF studio 7 always gives me an error that says:
Not able to open Device Control Panel For
Evaluation Board: Texas Instruments XDS100v3 A
RF Device: CC2538
Device ID: .......
Check if Evaluation Board is already in use by another tool.
Check jumpers on Evaluation Board
XDS100v3 only supports CJTAG and JTAG interfaces.
I just typed all this, can you tell me why is it asking me for the JTAG interfaces if I am using the USB cable?
Also, is there any way to edit the code that is in the board? to add stuff on top of it?