Part Number: LP-CC2651P3
Other Parts Discussed in Thread: LAUNCHXL-CC26X2R1, ENERGYTRACE
I have three types of development kits as belows.
1. LP-CC2651P3
2. LAUNCHXL-CC26X2R1
3. LAUNCHXL-CC1352P-2
I connect the XDS110 of these devices with jumper cables and use them to upgrade the firmware of the target device.
These devices are connected to a pc (Windows 10) via a usb cable.
When connecting the target device to the XDS110 for firmware upgrade, there is a problem that the USB driver is disconnected and reconnected.
This problem only occurs in LP-CC2651P3.
It doesn't happen in LAUNCHXL-CC26X2R1 and LAUNCHXL-CC1352P-2.
All XDS110 firmware versions are 3.0.0.20.
How can I solve this USB reconnection problem of LP-CC2651P3 ?