Part Number: CC2630
Other Parts Discussed in Thread: SYSBIOS, TIMAC, , Z-STACK
I'm writing for an application where using SYSBIOS in ROM isn't possible so I have to place a lot in flash. Unfortunately this has put me in a difficult situation resource wise, at the moment I do not have enough space to write my application in a way that can be updated over-the-air. A major factor is how much space is being taken by SYSBIOS and other IAR components.
I started by placing the stack image to the end of flash and applications will always reference it, that helped but wasn't enough. Looking at the map file:
Module ro code ro data rw data
------ ------- ------- -------
driverlib.lib: [6]
aon_batmon.o 40
chipinfo.o 36
cpu.o 24
ddi.o 162
driverlib_ver.o 1
flash.o 32
osc.o 528 20
setup.o 1 168
sys_ctrl.o 492 8
-----------------------------------------------------
Total: 2 482 29
drivers_cc26xxware.arm3: [7]
I2C.orm3 80 2 4
I2CCC26XX.orm3 1 128 20 20
PINCC26XX.orm3 956 220
UART.orm3 80
UARTCC26XX.orm3 1 812 40 16
-----------------------------------------------------
Total: 4 056 62 260
m7M_tl.a: [8]
DblAdd.o 232
DblCmpEq.o 32
DblCmpGe.o 46
DblCmpLe.o 46
DblDiv.o 598
DblMul.o 418
DblSub.o 384
DblToI32.o 88
I32ToDbl.o 48
pow.o 2 128
xdint.o 122
xdnorm.o 66
xdscale.o 268
xdtest.o 50
xexp.o 700
xlog.o 172
-----------------------------------------------------
Total: 5 398
rt7M_tl.a: [9]
ABImemclr.o 6
ABImemclr4.o 6
ABImemcpy_unaligned.o 118
ABImemset.o 102
ABImemset48.o 58
I64DivMod.o 238
I64DivZer.o 2
XXexit.o 12
data_init.o 40
lz77_init.o 450
memcmp_unaligned.o 98
strchr.o 22
strlen.o 54
zero_init3.o 64
-----------------------------------------------------
Total: 1 270
sysbios.arm3: [10]
BIOS.o 10 548 28
m3_Hwi_asm_iar.obj 272
m3_Hwi_asm_switch_iar.obj 104
m3_TaskSupport_asm_iar.obj 108
-----------------------------------------------------
Total: 11 032 28
Since these libraries aren't being actively developed anymore I think I could save some space by placing some of these outside my application. Is there any way to move some of this code to a fixed location in flash?