Other Parts Discussed in Thread: CC2530, Z-STACK
1. Problem description
A.Based on CC2530F256 hardware platform to develop air-conditioning energy-saving products (application scene base station room), there is an abnormal situation in the product operation (abnormal probability of 20%), after positioning, it is found that the FLASH internal program or data in CC2530F256 chip is inexplicably modified (different from the initial program segment data).
Abnormal comparison of B. FLASH data (abnormal on the left, normal on the right)

Note: The above is just an example. After analysis, the internal FLASH data of CC2530 of different products is randomly erased or abnormally changed, and the location of the erased FLASH is not fixed.
C.I hope to give some constructive and executable bug fixes.
2. Software framework design
Task scheduling management is based on ZigBee protocol stack OSAL, and some TI function modules are used to complete data acquisition and business processing functions.The engineering structure is shown in the figure below: