Hi,
I'm using the CC2530 with a custom board and, right now, the Z-Stack "GenericApp" for testing.
Everything works fine while debugging using the CC-Debugger and EW8051 (7.60.1). But, after unplugging the device from the debugger and resetting it (power-cycle or reset button), it stops running (no LED/UART/Wireless activity). I need to plug it into the Debugger (and sometimes unplug it again) and it starts working again. What could be the problem?