Part Number: CC1352P
Hi Ti!
Is an offset at the 27KHz RF frequency a large deviation or could it be considered acceptable?
Thanks very much
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC1352P
Hi Ti!
Is an offset at the 27KHz RF frequency a large deviation or could it be considered acceptable?
Thanks very much
Hi,
Are you measuring this on the 2.4 GHz port or on the sub-1 port ?
If your are measuring this at 2.440 GHz, then the offset is 11.1 ppm but if you are measuring this at 868 MHz, then the offset is 31.1 ppm.
The frequency offset should not exceed the maximum crystal offset of the crystal in ppm.