Part Number: CC2530
Hi,
Did get a question from a customer if we have done testing for ETSI EN 300 328 v2.2.2 on this device.
If we have, can we share the declaration of conformity?
Many thanks
Jorgen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC2530
Hi,
Did get a question from a customer if we have done testing for ETSI EN 300 328 v2.2.2 on this device.
If we have, can we share the declaration of conformity?
Many thanks
Jorgen
Hi Jörgen,
Yes, CC2530 is suitable for systems targeting ETSI EN 300 328. The DoC is available here: https://www.ti.com/lit/cr/sszqa24/sszqa24.pdf?ts=1700490227871&ref_url=https%253A%252F%252Fwww.ti.com%252Ftool%252FCC2530EMK
-Simon
Simon,
Was that the correct document, for me it's more related to: Directive 2011/65/EU Restriction of Hazardous Substances in Electrical and Electronic Equipment?
As far as I can see that document don't refer to the ETSI standard.
Br
Jorgen
Hi Jorgen,
I hope all is well. We currently do not have a signed DoC for the CC2350 EM that shows compliance to EN 300328 V2.2.2. The reason for this is that this is an older EVM and per TI compliance it is not required to test against the latest CE standard. Having said that, this part has been in production for sometime now and many customers have certified to the latest CE standard. We also state that this part is appropriate for CE per page 7 footnote (1) in the RF transmit section:
(1) Texas Instruments CC2530 EM reference design is suitable for systems targeting compliance with EN 300 328, EN 300 440, FCC CFR47 Part 15 and ARIB STD-T-66.
I hope this helps.
Thanks,
Riz