Hi All,
I have an issue with orphaned ZED. Once I take it away from its parent
(ZC in that case) and bring it closer (10cm) to other router on the network,
I see that ZED sends orphan notification and repeatedly sends beacons but,
it doesn't joins to the new parent. However, if am taking the device back to its
previous parent (the distance is ~5meters), the ZED joins back. What can be
the reason to such a behavior?
I'm using Z-Stack 2.4.0 (ZigBee-PRO), the part is cc2530 on a custom board.
The distance between ZC and ZR is ~10meters in office building like area.
The poll rates are managed manually as follows: The ZED switch the poll
rates from off to other intervals once it have some message to send.
After the message sent + few seconds all the poll rates switched back to
off state.
I've attached packet sniffer captures (cc2531 dongle): 3034.08.23.2011 - sniffer data.psd
- ZED NWK address is 0x182D.
- This behavior can bee seen from packet #154 to packet #233
If any one have an idea what is wrong here, please advice how can I fix
this behavior.
Edit:
In my last experiment, I've enabled NWK_AUTO_POLL, and removed
all lines of code where i'm manually setting the poll rates. Now when
ZED goes orphan it rejoins to network (added to a new parent).
Thank you in advance,
Igor