Part Number: CC2530-CC2592EM-RD
Other Parts Discussed in Thread: CC2592, CC2530
Hi Team i am looking for Antenna Design Pattern "CC2592 ,CC2530" For the below zigbee module and also share design files related to it .
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC2530-CC2592EM-RD
Other Parts Discussed in Thread: CC2592, CC2530
Hi Team i am looking for Antenna Design Pattern "CC2592 ,CC2530" For the below zigbee module and also share design files related to it .
Hi Narendar,
The antenna is a 2.4 GHz Inveted F antenna which can be found here: www.ti.com/.../swru120d.pdf
Here is the reference design for this design: https://www.ti.com/tool/TIDC-CC2530-CC2592EMK-RD
Best regards,
Bun
Hi the current module CC2530,CC2592 are having VQFN Packages .Is there any other Smaller packages other than this one and also is there any other module with the same specs with smaller packages kindly suggest if there are any
Hi Narender,
We do not have an IC can provide 20 dBm of output in a package size smaller than a 7x7mm which is what this device is and unfortunately using range extenders are limited to the CC25XX devices.
Best regards,
Bun