Part Number: CC2674P10
Other Parts Discussed in Thread: CC1354P10, , SYSCONFIG
Inputs:
- SDK version: 7_10_02_23
- CCS version: 12.2
- Firmware to reproduce selected: znp_LP_EM_CC1354P10_6_tirtos7_ticlang (this firmware is build for CC2674P10 RSK - important)
- Default pin settings RF:
- CONFIG_RF_24GHZ - DIO_34
- CONFIG_RF_HIGH_PA - DIO_3
- CONFIG_RF_SUB1GHZ - DIO_35
- Default pin settings peripheral:
- CONFIG_GPIO_RLED - DIO_6
- CONFIG_GPIO_GLED - DIO_7
- CONFIG_DISPLAY_UART (tx) - DIO_13
- CONFIG_DISPLAY_UART (rx) - DIO_12
- CONFIG_GPIO_BTN2 - DIO_14
- CONFIG_GPIO_BTN1 - DIO_15
- Default pin settings SPI:
- CONFIG_SPI_0 (poci) - DIO_37;
- CONFIG_SPI_0 (pico) - DIO_36;
- CONFIG_SPI_0 (sclk) - DIO_39;
- CONFIG_NVS_SPI_0 (chip select) - DIO_38;
- Default pin settings RF:
Aim:
- To compile firmware for hw board based on CC2674P10 RGZ that utilizes these pins:
- Required pin settings RF:
- CONFIG_RF_24GHZ - DIO_28
- CONFIG_RF_HIGH_PA - DIO_29
- CONFIG_RF_SUB1GHZ - DIO_30
- Required pin settings peripheral:
- CONFIG_GPIO_RLED - DIO_6
- CONFIG_GPIO_GLED - DIO_7
- CONFIG_DISPLAY_UART (tx) - DIO_13
- CONFIG_DISPLAY_UART (rx) - DIO_12
- CONFIG_GPIO_BTN2 - DIO_14
- CONFIG_GPIO_BTN1 - DIO_15
- Required pin settings SPI:
- CONFIG_SPI_0 (poci) - DIO_8;
- CONFIG_SPI_0 (pico) - DIO_9;
- CONFIG_SPI_0 (sclk) - DIO_10;
- CONFIG_NVS_SPI_0 (chip select) - DIO_20;
- Required pin settings RF:
I need to try standard firmware from SDK on the chip CC2674P10 RGZ version. So basically, i need to change pins for RF only, because i am not going to use SPI in my project. In RF, i amnot ineterested in sub 1Ghz, so need only update pins ...RF_24GHZ and ...RF_HIGH_PA.
Steps to reproduce:
- Create new project (CCS -> Import -> CCS Projects -> (Examples\Rtos folder from SDK) -> znp_LP_EM_CC1354P10_6_tirtos7_ticlang
- Open znp.syscfg
- Show device view
- Switch the device and change the chip to CC2674P10 RGZ switch-device.jpg
- Generic errors appear, but you can accept them: generic-errors.jpg
- Change RF pins to DIO_28 and DIO_29
- Error re RF appears, you can't ignore it: rf-errors.jpg
- Build firmware
- Errors during compiling
- - logs is here logs.txt
- - errors summary errors-summary.jpg
Question:
- How to build default firmware znp_LP_EM_CC1354P10_6_tirtos7_ticlang
for chip CC2674P10 RGZ (7*7 48 GPIOs)
while SDK's template is only for CC2674P10 RSK (8*8 64 GPIOs)?