This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2531: Using an external 32MHz oscillator, do I need to do anything with the XOSC_Q2 pin?

Part Number: CC2531


I am using the CC2531 with an external 32MHz oscillator connected to to XOSC_Q1 (pin 22).  Do I need to anything with XOSC_Q2 (pin 23)?  For example, I know that some chips require grounding the other clock pin when using an external oscillator (as opposed to a crystal).

Thanks