Hi guys,
I am interested in using the Channel inteference detection and resolution feature provided by Zstack 2.4 , everything about it is understood by me in the description provided in the Zstack Developer's Guide.pdf
But a couple of things is unclear because of the way my application is implemented
1) On Channel interference detection at the router/endevice does it do a scan on all channels or only those channels that is defined by the channel mask
2) On the Coordinator side also can it select a Channel which is not defined by the local channel mask
All other conditions being satisfied is this possible?