Hi,
Well am in middle of testing the whole pan id conflict detection and resolution functionality , as per the documentation (Z-Stack Developer's Guide ) it says that if a node detects a beacon the process is initiated. Well in my test setup i want to have two coordinator both on the programmed for the same channel no and panid and aslo both have the NWK_MANAGER flag compiled .
Both coordinators are started at the same time , this is what happens, one coordinator forms the network on the panid and sends a becon which is received by the other coordinator on which i get the following frames thats seen on the sniffer.
Both the panid were set to 0x1234 although the last frame was destined to 0x1235 what does that mean and did either of the coordinator change its panid?
P.S sorry about the image been abt the text :)