This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2674R10: Zigbee OTA

Part Number: CC2674R10
Other Parts Discussed in Thread: LP-CC2652R7, , CC2652R7

Tool/software:

Hi Team, 

The OTA Academy states : "On-chip OAD is only supported by the LP-CC2652R7 or LP-CC1352P7-4". 

However I saw zc_ota_server working with the CC2674R10. 

-> Can you confirm the Academy also works with the CC2674x10 ? 

Thanks

Geoffrey

  • Hi Geoffrey,

    Correct, more generally no Zigbee OTA clients exist for CC13x4/CC26x4 devices.

    These may exist in the future, but in the meantime it is possible to implement based on:

    • CC13x2/CC26x2 Zigbee OTA client example
    • CC13x4/CC26x4 BLE OTA on-chip example

    Could you consider using CC2652R7?
    Is the CC26x4 needed because more flash is required?

    Thanks,
    Toby