Part Number: CC2652R
Tool/software:
Hello,
We have an application that uses the SimpleLink CC13x2 26x6 SDK v4.20.01.04. We recently added a few custom nonvol tokens using the OSAL SNV system. We have two tokens in particular that are large structures - about 110 bytes each with potential to grow a little more in the future. From a document here, in Listing 30, it sounds like our application tokens must use ID values between 0x80 and 0x8F. Is that correct?
Today I ran across a bunch of NV item IDs in the zcomdef.h file (lines 212-226), including the following:
- #define ZCD_NV_LEGACY_NWK_SEC_MATERIAL_TABLE_END 0x0080
- #define ZCD_NV_USERDESC 0x0081
- #define ZCD_NV_NWKKEY 0x0082
- #define ZCD_NV_PANID 0x0083
- #define ZCD_NV_CHANLIST 0x0084
- #define ZCD_NV_LEAVE_CTRL 0x0085
- #define ZCD_NV_SCAN_DURATION 0x0086
- #define ZCD_NV_LOGICAL_TYPE 0x0087
- #define ZCD_NV_NWKMGR_MIN_TX 0x0088
- #define ZCD_NV_NWKMGR_ADDR 0x0089
- #define ZCD_NV_ZDO_DIRECT_CB 0x008F
Obviously, this made me question my understanding from the documentation that we could use the NV token ID space from 0x80 to 0x8F and not have any conflicts. It seems that writing to my tokens with ID 0x80, 0x81, 0x82, etc could very well be conflicting with these and causing corruption, right?
If that is the case, is there an ID space I can use for my application tokens that will not run into conflicts with the stack? This file has dozens of token IDs, and some seem to overlap each other too (ZCD_NV_EX_ADDRMGR, ZCL_PORT_SCENE_TABLE_NV_ID, ZCD_NV_EXTADDR all == 0x0001). What am I misunderstanding about the documentation and the OSAL SNV ID system?
Thanks,
Damon