Part Number: CC2531EMK
Tool/software:
Can you please provide the FW for CC2531-F128 zigbe dongle , & drivers
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi sowmya,
Please download Z-Stack v3.0.2, there are pre-build resources located here:
CC2531ZNP-without-SBL.bin: \Projects\zstack\ZNP\CC253x\dev
ccxxxx_usb_cdc.cat/.int: \Components\hal\target\CC2530USB\usb\drive
The CC2531EMK features the CC2531F256 and as such all pre-built versions are intended only for this version of the device. Further user development is required to support other flash memory versions. Other CC USB Firmware Library and Examples are available from SWRC088.
Regards,
Ryan