Part Number: CC2652P
Tool/software:
Is there a recommended MAX_RTG_ENTRIES value for a network size of 200? The network is consist of 32 routers and 168 end devices, what value should be used to have a steady network?
Best regards,
Shuyang
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC2652P
Tool/software:
Is there a recommended MAX_RTG_ENTRIES value for a network size of 200? The network is consist of 32 routers and 168 end devices, what value should be used to have a steady network?
Best regards,
Shuyang
Hello Shuyang Zhong,
I think we could first test with 200 as the max value (note that there are two types of tables one is large and the other smaller, the threshold is 255), and then tune it down to see if performance decreases, though central should keep the size of 200 (or greater).

Thanks,
Alex F