Hello, i have the cc2530ZNP mini development kit,I want to know if someone knows how to send data from coordinator to end device and works well.
I'm trying, sometimes send data and turns on a Led of the end device, but the second time that i send something, the coordinator reset (error -31) and lost the connection with the end device.i think that the end device don't send the af_data_confirm but i don't sure and i don't know fix.
also like to know if there is any function that say which device are linked to the network.
My last question is if anyone knows how to use the ZNP in linux to read the serial port, I have tried with GTKTERM, but did not detect the device
thanks.