Hello! I have the following problem: I can not do "over air download" (I'm using the latest version and cc2530 zstack, doing everything according to instructions)
1) Uploading Boot.eww
2) Uploading GenericApp.eww
3) On the other chip load Doongle.eww
4) is connected to a computer this card and run ZOAD.exe
5) connected to the network, which was created by GenericApp
6) I see that thedevices are marked with black (hence there is a Boot)
7) Opt for a generated file .bin and try to reflash
8) But! After some time, writes: Store image time out
Can you help me?