Part Number: CC2538-CC2592EMK
Other Parts Discussed in Thread: CC2538
Tool/software:
hi team,
i am working with cc2538 am using external SPI flash IS25LP128 so how can i congifure for read and write operation and also suggest refrance code for that
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC2538-CC2592EMK
Other Parts Discussed in Thread: CC2538
Tool/software:
hi team,
i am working with cc2538 am using external SPI flash IS25LP128 so how can i congifure for read and write operation and also suggest refrance code for that
Hello Mayur,
With the CC2538 I believe you will need to download IAR or use flash programmer. On the product page of the cc2538 the driverlib should have the SPI library in CC2538 Foundation Firmware download.
Thanks,
Alex F
#define SPI_PIN_SSI_CLK GPIO_PIN_6 // PC6
#define SPI_PIN_SSI_CS GPIO_PIN_7 // PC7
#define SPI_PIN_SSI_DO GPIO_PIN_3 // PD3
#define SPI_PIN_SSI_DI GPIO_PIN_5 // PD5
#define SPI_PIN_SSI_WP GPIO_PIN_7 // PA7
#define SPI_PIN_SSI_HOLD GPIO_PIN_6 // PA6
#define SPI_GPIO_SSI_BASE_CLK_CS GPIO_C_BASE // PC6, PC7
#define SPI_GPIO_SSI_BASE_DO_DI GPIO_D_BASE // PD3, PD5
#define SPI_GPIO_SSI_BASE_WP_HOLD GPIO_A_BASE // PA7, PA6
i am define this pin for my SPI flash using SSI pins is it correct
Hello Mayur Savalgi,
You may need to run some tests on your own custom configuration of SPI but the SPI example uses:
#define EXAMPLE_PIN_SSI_CLK GPIO_PIN_2
#define EXAMPLE_PIN_SSI_FSS GPIO_PIN_3
#define EXAMPLE_PIN_SSI_RX GPIO_PIN_4
#define EXAMPLE_PIN_SSI_TX GPIO_PIN_5
/******************************************************************************
* Filename: spi_master.c
* Revised: $Date: 2013-04-10 11:13:39 +0200 (Wed, 10 Apr 2013) $
* Revision: $Revision: 9701 $
*
* Description: Example demonstrating how to configure SSI0 in SPI master
* mode.
*
* Copyright (C) 2013 Texas Instruments Incorporated - http://www.ti.com/
*
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
******************************************************************************/
#include <stdbool.h>
#include <stdint.h>
#include "hw_memmap.h"
#include "hw_ioc.h"
#include "gpio.h"
#include "ioc.h"
#include "ssi.h"
#include "uart.h"
#include "sys_ctrl.h"
#include "uartstdio.h"
//
// NOTE:
// This example has been run on a SmartRF06 evaluation board.
// Short the Tx (PA5) and Rx (PA4) pins together.
// The code sends data on the Tx line and with the Tx and Rx pins shorted
// you are creating a loopback. The code then verifies that the data you
// received matches the code that you sent out. Use the terminal window
// to see the results of the data sent and received.
//
//*****************************************************************************
//
//! \addtogroup ssi_examples_list
//! <h1>SPI Master (spi_master)</h1>
//!
//! This example shows how to configure the SSI0 as SPI Master. The code will
//! send three characters on the master Tx then polls the receive FIFO until
//! 3 characters are received on the master Rx.
//!
//! This example uses the following peripherals and I/O signals. You must
//! review these and change as needed for your own board:
//! - SSI0 peripheral
//! - GPIO Port A peripheral (for SSI0 pins)
//! - SSI0Clk - PA2
//! - SSI0Fss - PA3
//! - SSI0Rx - PA4
//! - SSI0Tx - PA5
//!
//! The following UART signals are configured only for displaying console
//! messages for this example. These are not required for operation of SSI0.
//! - UART0 peripheral
//! - GPIO Port A peripheral (for UART0 pins)
//! - UART0RX - PA0
//! - UART0TX - PA1
//!
//! This example uses the following interrupt handlers. To use this example
//! in your own application you must add these interrupt handlers to your
//! vector table.
//! - None.
//
//*****************************************************************************
#define EXAMPLE_PIN_SSI_CLK GPIO_PIN_2
#define EXAMPLE_PIN_SSI_FSS GPIO_PIN_3
#define EXAMPLE_PIN_SSI_RX GPIO_PIN_4
#define EXAMPLE_PIN_SSI_TX GPIO_PIN_5
#define EXAMPLE_GPIO_SSI_BASE GPIO_A_BASE
#define EXAMPLE_PIN_UART_RXD GPIO_PIN_0
#define EXAMPLE_PIN_UART_TXD GPIO_PIN_1
#define EXAMPLE_GPIO_UART_BASE GPIO_A_BASE
//*****************************************************************************
//
// Number of bytes to send and receive.
//
//*****************************************************************************
#define NUM_SSI_DATA 3
//*****************************************************************************
//
// This function sets up UART0 to be used for a console to display information
// as the example is running.
//
//*****************************************************************************
void
InitConsole(void)
{
//
// Map UART signals to the correct GPIO pins and configure them as
// hardware controlled.
//
IOCPinConfigPeriphOutput(EXAMPLE_GPIO_UART_BASE, EXAMPLE_PIN_UART_TXD,
IOC_MUX_OUT_SEL_UART0_TXD);
GPIOPinTypeUARTOutput(EXAMPLE_GPIO_UART_BASE, EXAMPLE_PIN_UART_TXD);
IOCPinConfigPeriphInput(EXAMPLE_GPIO_UART_BASE, EXAMPLE_PIN_UART_RXD,
IOC_UARTRXD_UART0);
GPIOPinTypeUARTInput(EXAMPLE_GPIO_UART_BASE, EXAMPLE_PIN_UART_RXD);
//
// Initialize the UART (UART0) for console I/O.
//
UARTStdioInit(0);
}
//*****************************************************************************
//
// Configure SSI0 in master Freescale (SPI) mode. This example will send out
// 3 bytes of data, then wait for 3 bytes of data to come in. This will all be
// done using the polling method.
//
//*****************************************************************************
int
main(void)
{
uint32_t pui32DataTx[NUM_SSI_DATA];
uint32_t pui32DataRx[NUM_SSI_DATA];
uint32_t ui32Index;
//
// Set the clocking to run directly from the external crystal/oscillator.
// (no ext 32k osc, no internal osc)
//
SysCtrlClockSet(false, false, SYS_CTRL_SYSDIV_32MHZ);
//
// Set IO clock to the same as system clock
//
SysCtrlIOClockSet(SYS_CTRL_SYSDIV_32MHZ);
//
// Set up the serial console to use for displaying messages. This is
// just for this example program and is not needed for SSI operation.
//
InitConsole();
//
// Display the setup on the console.
//
UARTprintf("SSI ->\n");
UARTprintf(" Mode: SPI\n");
UARTprintf(" Data: 8-bit\n\n");
//
// The SSI0 peripheral must be enabled for use.
//
SysCtrlPeripheralEnable(SYS_CTRL_PERIPH_SSI0);
//
// Disable SSI function before configuring module
//
SSIDisable(SSI0_BASE);
//
// Set IO clock as SSI clock source
//
SSIClockSourceSet(SSI0_BASE, SSI_CLOCK_PIOSC);
//
// For this example SSI0 is used with PA2-PA5. The actual port and pins
// used may be different on your part, consult the data sheet for more
// information. GPIO port A needs to be enabled so these pins can be used.
// TODO: change this to whichever GPIO port you are using.
//
// Configure the pin muxing for SSI0 functions on port A2, A3, A4, and A5.
// This step is not necessary if your part does not support pin muxing.
// TODO: change this to select the port/pin you are using.
//
IOCPinConfigPeriphOutput(EXAMPLE_GPIO_SSI_BASE, EXAMPLE_PIN_SSI_CLK,
IOC_MUX_OUT_SEL_SSI0_CLKOUT);
IOCPinConfigPeriphOutput(EXAMPLE_GPIO_SSI_BASE, EXAMPLE_PIN_SSI_FSS,
IOC_MUX_OUT_SEL_SSI0_FSSOUT);
IOCPinConfigPeriphOutput(EXAMPLE_GPIO_SSI_BASE, EXAMPLE_PIN_SSI_TX,
IOC_MUX_OUT_SEL_SSI0_TXD);
IOCPinConfigPeriphInput(EXAMPLE_GPIO_SSI_BASE, EXAMPLE_PIN_SSI_RX,
IOC_SSIRXD_SSI0);
//
// Configure the GPIO settings for the SSI pins. This function also gives
// control of these pins to the SSI hardware. Consult the data sheet to
// see which functions are allocated per pin.
// The pins are assigned as follows:
// PA5 - SSI0Tx
// PA4 - SSI0Rx
// PA3 - SSI0Fss
// PA2 - SSI0CLK
// TODO: change this to select the port/pin you are using.
//
GPIOPinTypeSSI(EXAMPLE_GPIO_SSI_BASE, EXAMPLE_PIN_SSI_CLK |
EXAMPLE_PIN_SSI_FSS | EXAMPLE_PIN_SSI_RX |
EXAMPLE_PIN_SSI_TX);
GPIOPinTypeSSI(EXAMPLE_GPIO_SSI_BASE, EXAMPLE_PIN_SSI_CLK |
EXAMPLE_PIN_SSI_RX | EXAMPLE_PIN_SSI_TX);
//
// Configure SSI module to Motorola/Freescale SPI mode 3:
// Polarity = 1, SCK steady state is high
// Phase = 1, Data changed on first and captured on second clock edge
// Word size = 8 bits
//
SSIConfigSetExpClk(SSI0_BASE, SysCtrlIOClockGet(), SSI_FRF_MOTO_MODE_3,
SSI_MODE_MASTER, SysCtrlClockGet()/2, 8);
//
// Enable the SSI0 module.
//
SSIEnable(SSI0_BASE);
//
// Read any residual data from the SSI port. This makes sure the receive
// FIFOs are empty, so we don't read any unwanted junk. This is done here
// because the SPI SSI mode is full-duplex, which allows you to send and
// receive at the same time. The SSIDataGetNonBlocking function returns
// "true" when data was returned, and "false" when no data was returned.
// The "non-blocking" function checks if there is any data in the receive
// FIFO and does not "hang" if there isn't.
//
while(SSIDataGetNonBlocking(SSI0_BASE, &pui32DataRx[0]))
{
}
//
// Initialize the data to send.
//
pui32DataTx[0] = 's';
pui32DataTx[1] = 'p';
pui32DataTx[2] = 'i';
//
// Display indication that the SSI is transmitting data.
//
UARTprintf("Sent:\n ");
//
// Send 3 bytes of data.
//
for(ui32Index = 0; ui32Index < NUM_SSI_DATA; ui32Index++)
{
//
// Display the data that SSI is transferring.
//
UARTprintf("'%c' ", pui32DataTx[ui32Index]);
//
// Send the data using the "blocking" put function. This function
// will wait until there is room in the send FIFO before returning.
// This allows you to assure that all the data you send makes it into
// the send FIFO.
//
SSIDataPut(SSI0_BASE, pui32DataTx[ui32Index]);
}
//
// Wait until SSI0 is done transferring all the data in the transmit FIFO.
//
while(SSIBusy(SSI0_BASE))
{
}
//
// Display indication that the SSI is receiving data.
//
UARTprintf("\nReceived:\n ");
//
// Receive 3 bytes of data.
//
for(ui32Index = 0; ui32Index < NUM_SSI_DATA; ui32Index++)
{
//
// Receive the data using the "blocking" Get function. This function
// will wait until there is data in the receive FIFO before returning.
//
SSIDataGet(SSI0_BASE, &pui32DataRx[ui32Index]);
//
// Since we are using 8-bit data, mask off the MSB.
//
pui32DataRx[ui32Index] &= 0x00FF;
//
// Display the data that SSI0 received.
//
UARTprintf("'%c' ", pui32DataRx[ui32Index]);
}
//##### SELF CHECK BEGIN #####
//
// Check that the data you sent was the same as the data that you received.
//
for(ui32Index = 0; ui32Index < NUM_SSI_DATA; ui32Index++)
{
if(pui32DataTx[ui32Index] != pui32DataRx[ui32Index])
{
//
// Tell the user that the test failed.
//
UARTprintf("\n\nError: Data does not exactly match.\n");
UARTprintf("Check that Tx & Rx are shorted together.\n\n");
//
// Wait in infinite loop for debugging.
//
while(1)
{
}
}
}
//
// Tell the user that the test passed.
//
UARTprintf("\n\nTest Passed.\n\n");
//##### SELF CHECK END #####
//
// Done - enter an infinite loop.
//
while(1)
{
}
}
Thanks,
Alex F