Part Number: CC2674P10
Other Parts Discussed in Thread: CC2674R10,
Tool/software:
Hi,
It is difficult to predict the erasing time of an internal flash section : the datasheet gives 2.1ms typical at 0 cycle and 4s maximum at 30K cycle.

-> Is it possible to have more typical information for other values across that range ? at 10K for example ?
Also, the CC2674R10 datasheet indicates 10ms typical at 0 cycle. Iassume it is a mistake ?

Thanks
Geoffrey