Hello all,
I'm currently trying to use binding to establish communication between 2 devices. I'm using the end device bind function and I get a bind success message. So it appears to me that binding is successful. However, I then attempt to use afSendData to send communications between the two devices. What I can't figure out is that my transmissions work perfectly if I do a broadcast, but if I use 0xFFFE for the destAddr to tell it to use the binding table then no message is ever transmitted. (I'm watching the transmissions with a packet sniffer and I can see all other messages that I send). I'm assuming I'm doing something wrong when I go to transmit the message, or perhaps when I execute the binding itself? I was wondering if anyone could tell me which direction to look. Let me know if you need more data from me. I will be happy to provide.
Thanks