CC2652R: DMM with Ble Peripheral + Ti15.4 Coordinator - transmit on top of transmit assert triggered
Tool/software:
Hi!
I want to follow up on my previous thread (CC2652R: DMM with Ble Peripheral + Ti15.4 Coordinator - transmit on top of transmit assert triggered - Zigbee & Thread forum - Zigbee & Thread - TI E2E support forums).
Running my project with some additional debug output I was able to get the LR value at the time of assert. Using addr2line tool here is where the LR points to:
/home/developer/.conan/data/ti154stack/6.41.00.07/library-lprf/ga/build/c90184d484f3f95c6a6179391966efa64b8ab8fe/source/ti/ti154stack/low_level/cc13xx/mac_tx.c:329
Unfortunately this file is not available in source in simplelink_cc13xx_cc26xx_sdk_7_41_00_17 so I hope to get an answer what is this assert and how can I debug it further (without access to source files) to prevent it from happening?
Hello,
I just installed the internal, source SDK for the 7.41.00.17 SDK.
In the mac_tx.c, I see this near line 329:
Not entirely sure this is giving more info to your error.
Can you possibly trigger this same error more quickly if you introduce more noise into the environment?
Thanks,
Toby