Hi ,
I am using the latest release software ZStack-CC2530-2.5.0 . I am testing the MT commands with 2 devices one Coordinator and one Router.
The Coordinator is connected to Z-tools . Using the TI Sniffer i am able to find the Router Network ID.
Using Z-tools i gave ZDO_MGMT_LQI_REQ commands with parameters 0xDAFE as network id and 0 as start index. I got the response but unable to see the LQI value.
<TX>11:37:54.99 COM12 ZDO_MGMT_LQI_REQ (0x2531)
DstAddr: 0xDAFE
StartIndex: 0x00
<RX>11:37:55.01 COM12 ZDO_MGMT_LQI_REQ_SRSP (0x6531)
Status: afStatus_SUCCESS (0x0)
kindly advice.
Thanks and Regards
Lakshman.