This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1352P: Issue: Router crashes when join into the network.

Part Number: LAUNCHXL-CC1352P

Tool/software:

There are multiple coordinators in the environment, all of whom have closed the Permit Job. If the router fails to detect the possibility of joining the network, it will crash.

it is. This issue is caused by the function 'bdb_filterNwkDisc'. It can be fixed like this.

void bdb_filterNwkDisc(void)
{
  networkDesc_t* pNwkDesc;
  uint8_t i = 0;
  uint8_t ResultCount = 0, ResultTotal = 0;

  pBDBListNwk  = nwk_getNwkDescList();
  nwk_desc_list_release();

  pNwkDesc = pBDBListNwk;
  while (pNwkDesc)
  {
    ResultCount++;
    pNwkDesc = pNwkDesc->nextDesc;
  }

  ResultTotal = ResultCount;

  if(pBDBListNwk)
  {
    pNwkDesc = pBDBListNwk;

    if(pNwkDesc)
    {
      void *nextDesc = pNwkDesc->nextDesc;
      // "nextDesc" replace "pNwkDesc->nextDesc" because "pNwkDesc->nextDesc" is not corret after freed, fixed by LuoYiming 2025-03-10
      for ( i = 0; i < ResultTotal; i++, pNwkDesc = nextDesc ) 
      {
        nextDesc = pNwkDesc->nextDesc; // get the "nextDesc" before "pNwkDesc" is freed, fixed by LuoYiming 2025-03-10
        if ( nwk_ExtPANIDValid( ZDO_UseExtendedPANID ) == true )
        {
          // If the extended Pan ID is commissioned to a non zero value
          // Only join the Pan that has match EPID
          if ( osal_ExtAddrEqual( ZDO_UseExtendedPANID, pNwkDesc->extendedPANID) == false )
          {
            //Remove from the list
            bdb_nwkDescFree(pNwkDesc);
            ResultCount--;
            continue;
          }
        }
        else if ( zgConfigPANID != 0xFFFF )
        {
          // PAN Id is preconfigured. check if it matches
          if ( pNwkDesc->panId != zgConfigPANID )
          {
            //Remove from the list
            bdb_nwkDescFree(pNwkDesc);
            ResultCount--;
            continue;
          }
        }

        if ( pNwkDesc->chosenRouter != _NIB.nwkCoordAddress || _NIB.nwkCoordAddress == INVALID_NODE_ADDR )
        {
          // check that network is allowing joining
          if ( ZSTACK_ROUTER_BUILD )
          {
            if ( !pNwkDesc->routerCapacity )
            {
              //Remove from the list
              bdb_nwkDescFree(pNwkDesc);
              ResultCount--;
              continue;
            }
          }
          else if ( ZSTACK_END_DEVICE_BUILD )
          {
            if ( !pNwkDesc->deviceCapacity )
            {
              //Remove from the list
              bdb_nwkDescFree(pNwkDesc);
              ResultCount--;
              continue;
            }
          }
        }

        // check version of zigbee protocol
        if ( pNwkDesc->version != _NIB.nwkProtocolVersion )
          continue;

        // check version of stack profile, only matching profiles are supported
        if ( pNwkDesc->stackProfile != zgStackProfile  )
        {
            //Remove from the list
            bdb_nwkDescFree(pNwkDesc);
            ResultCount--;
            continue;
        }
      }
    }
  }

  //Notify the application about the remaining valid networks to join
  if(pfnFilterNwkDesc)
  {
    pfnFilterNwkDesc(pBDBListNwk, ResultCount);
  }
}