This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652P: same callback functions for different endpoints

Part Number: CC2652P
Other Parts Discussed in Thread: CC1354P10,

Tool/software:

My device has several endpoints which all have the same on/off function. Starting from the zed_lights example, I have done:

zclGeneral_RegisterCmdCallbacks( HYDRONIC_VALVULES_ENDPOINT1, &zclHydronicController_CmdCallbacks );
zclGeneral_RegisterCmdCallbacks( HYDRONIC_VALVULES_ENDPOINT2, &zclHydronicController_CmdCallbacks2 );
static zclGeneral_AppCallbacks_t zclHydronicController_CmdCallbacks =
{
  zclHydronicController_BasicResetCB,            // Basic Cluster Reset command
  NULL,                                   // Identfiy cmd
  NULL,                                   // Identify Query command
  zclHydronicController_IdentifyQueryRspCB,      // Identify Query Response command
  NULL,                                   // Identify Trigger Effect command
#ifdef ZCL_ON_OFF
  zclHydronicValvules1_OnOffCB,                 // On/Off cluster commands
  NULL,                                   // On/Off cluster enhanced command Off with Effect
  NULL,                                   // On/Off cluster enhanced command On with Recall Global Scene
  NULL,                                   // On/Off cluster enhanced command On with Timed Off
#endif
#ifdef ZCL_LEVEL_CTRL
  zclHydronicController_LevelControlMoveToLevelCB,             // Level Control Move to Level command
  zclHydronicController_LevelControlMoveCB,                    // Level Control Move command
  zclHydronicController_LevelControlStepCB,                    // Level Control Step command
  zclHydronicController_LevelControlStopCB,                    // Level Control Stop command
  zclHydronicController_LevelControlMoveToClosestFrequencyCB,  // Level Control Stop command
#endif
#ifdef ZCL_GROUPS
  NULL,                                   // Group Response commands
#endif
#ifdef ZCL_SCENES
  zclHydronicController_SceneStoreCB,           // Scene Store Request command
  zclHydronicController_SceneRecallCB,          // Scene Recall Request command
  NULL,                                  // Scene Response command
#endif
#ifdef ZCL_ALARMS
  NULL,                                  // Alarm (Response) commands
#endif
#ifdef SE_UK_EXT
  NULL,                                  // Get Event Log command
  NULL,                                  // Publish Event Log command
#endif
  NULL,                                  // RSSI Location command
  NULL                                   // RSSI Location Response command
};
However, even if endpoint 2 is called, always the function registered for the first endpoint will be called.
Any idea why this could happen? Even if this would work correctly, is there a more elegant way by passing the endpoint as parameter of the callback functions so that I do not need to duplicate functions?
Thank you and regards
Peter
PS: the module is actually CC1354P10 and not CC2652P but when selecting the right module, I cannot post into the ZigBee forum...