Part Number: LP-CC2652R7
Other Parts Discussed in Thread: CC2652R7, ENERGYTRACE
Tool/software:
Good morning,
I am working with two LP-CC2652R7 boards using the Green Power Device example from the SimpleLink SDK 8.30.01.01. One board runs the gp_switch project, and the other runs gp_sink_light.
I successfully completed the commissioning process between the two devices. Then, I measured the current consumption of the gp_switch device using EnergyTracer (not in debugger mode). However, I am seeing a minimum current draw of around 0.1 mA, which seems too high for a Green Power device.
Setup details:
-
I removed all LaunchPad jumpers except GND, 3.3V, and RESET.
-
I defined the
CUI_DISABLEmacro in thegp_switchproject to disable the UART interface. -
The device was tested standalone, outside of debug mode.
My questions are:
-
Is this ~0.1 mA current draw expected for the
gp_switchexample? -
Are there any additional modifications or configurations required to achieve ultra-low power consumption as intended for Green Power devices?
-
Based on the EnergyTracer results, it seems the device would not be able to operate autonomously for long. Is this normal for this example, or are there further optimizations to apply?
Any guidance or suggestions would be greatly appreciated. I can also provide images from the EnergyTracer output if needed.
Best regards,
1er case: Not sendig GPDFs


2do case: Sending GPDFs