This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R5: An SDK installation problem occurred

Part Number: CC2340R5

Tool/software:

SDk:  simplelink_lowpower_f3_sdk_9_10_00_83.exe

windows: Windows 10 64bit

I chose to ignore this problem and continue with the installation. I then imported the example project C:\ti\simplelink_lowpower_f3_sdk_9_10_00_83\examples\rtos\LP_EM_CC2340R5\zigbee\onoff_switch,  and was prompted with the following problems


I installed ti_cgt_armllvm_4.0.2.LTS_windows-x64_installer.exe according to the prompt, but it didn't  work