Part Number: CC2530
Tool/software:
Hello,
I use Digi XBee Pro moduls and send frames in the format shown in the picture below:

I would like to use TI modules and I am asking for help in choosing. The systems are powered by batteries, so it would be good if they had low power consumption and allowed data transmission at a distance of up to 100 m. The devices work in a Mesh network, and the recipient/sender address, data length and data up to 20 bytes are sent.
Thank you for your help