This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652RB: CC2652RB - Lean Layout check

Part Number: CC2652RB

Tool/software:

Hi all,

playing around with my latest iteration of a zigbee hub

and try to make it lean as possible.

The question here is, that I have ripped out the oscillators because according to the datasheet its not mandatory to have one,
if I dont plan to have the zigbee stick on a low standby mode.



Also the Antenna is a low dBi Antenna - is that also correct ?

BR

  • Hi,

    The question here is, that I have ripped out the oscillators because according to the datasheet its not mandatory to have one,
    if I dont plan to have the zigbee stick on a low standby mode.

    Yes, this is correct. The 48 MHz and the 32 kHz crystals are not needed under the conditions above.  

    Also the Antenna is a low dBi Antenna - is that also correct ?

    The choice of an antenna is entirely up to your design constraints of space and desired gain. I strongly recommend reading the AN058 – Antenna Selection Guide for additional considerations on the antenna selection. 

    Hope this helps,

    Rafael