Part Number: CC2650STK
Other Parts Discussed in Thread: CC1352R, CC2650
Tool/software:
Hi there,
As part of a research project, we have purchased 17 units of the CC2650STK Sensortag. We are planning to run Contiki-NG in TSCH mode on these devices.
When I flash the device, I would like to read the Contiki-NG serial (print) output from my laptop, just as I do with my CC1352R SensorTag devices.
I see that the device has a DevPack Connector, specifically a Samtec Inc. LSS-110-01-F-DV-A-TR model, and I noticed UART_TX and UART_RX pins on it. However, I couldn’t determine whether this connector is male or female.
My Questions:
-
Would it be appropriate to buy a connector like the following and manually solder cables to access UART or is there any other useful products?
-
I also need to perform digital input reading from the external environment. Is the DevPack connector the only way to interface with digital inputs as well?
Thanks in advance for your help!
Best regards,
İsmail Hakkı TURAN
ismailhakkituran.github.io/