Part Number: CC2530
Tool/software:
Hello
I am using the CC2530 as a ZED and the CC2652 as ZC. Currently, there is one ZC and one ZED placed very close to each other. During testing, I found that when the ZED continuously sends data every 50ms (4 bytes per packet), it works fine. However, if the interval is reduced to 40ms, ZR receive packet loss occurs. Does Zigbee communication require a fixed minimum interval, or could this be an issue with the hardware or firmware?