Part Number: CC2652P
Other Parts Discussed in Thread: CC1352P, , ,
Tool/software:
Hello
I'm using the Zigbee End Device Switch example to test my custom board which uses E72-2G4M20S1E (C2652P)
My coordinator is Raspberry Pi running Zigbee2Mqtt
The failure is "Interview failed because can not get node descriptor"
I also sniffed the network and see that the following - it looks like the coordinator asks my device for Node Descriptor Request - and after timeout of 1 minute it gives up
I suspect it may a security issue - since I can't view properly the device message on Wireshark
I'm attaching the sniffer file too
Thanks
Haim
11 27.241174 00:12:4b:00:26:d0:f0:d7 0x0000 IEEE 802.15.4 19 Association Request, RFD
12 27.242230 IEEE 802.15.4 3 Ack
13 27.611772 00:12:4b:00:26:d0:f0:d7 0x0000 IEEE 802.15.4 16 Data Request
14 27.612732 IEEE 802.15.4 3 Ack
15 27.614747 00:12:4b:00:2c:3a:31:ea 00:12:4b:00:26:d0:f0:d7 IEEE 802.15.4 25 Association Response, PAN: 0x9a0b Addr: 0x88a6
16 27.615995 IEEE 802.15.4 3 Ack
17 27.618639 0x88a6 0x0000 ZigBee 54 Command, Dst: 0x0000, Src: 0x88a6
18 27.620815 IEEE 802.15.4 3 Ack
19 27.755205 0x88a6 Broadcast ZigBee 55 Data, Dst: Broadcast, Src: 0x88a6
20 27.757413 IEEE 802.15.4 3 Ack
21 27.848985 0x88a6 0x0000 IEEE 802.15.4 10 Data Request
22 27.849753 IEEE 802.15.4 3 Ack
23 28.271559 0x88a6 0x0000 IEEE 802.15.4 10 Data Request
24 28.272326 IEEE 802.15.4 3 Ack
25 28.274974 0x0000 0x88a6 ZigBee 71 Transport Key
26 28.277695 IEEE 802.15.4 3 Ack
27 28.375566 0x88a6 0x0000 IEEE 802.15.4 10 Data Request
28 28.376334 IEEE 802.15.4 3 Ack
29 28.385335 0x0000 0x88a6 ZigBee ZDP 46 Node Descriptor Request, Nwk Addr: 0x88a6
30 28.385000 IEEE 802.15.4 3 Ack
31 28.470070 0x88a6 0x0000 IEEE 802.15.4 10 Data Request