Part Number: CC2340R5
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
In a previous message it was said that Texas was aware of an issue in SimpleLink F3 SDK v9.11 that prevents the poll rate going above 5s and that it would be solved in the next release.
I am using SimpleLink F3 SDK v9.12 and would like to set a poll period larger than 5 seconds but it did not work,setting larger values in SysConfig, the maximum period that works is 5s in my case. I tried the suggested workaround calling zb_zdo_pim_set_long_poll_interval() with larger values in application but it also did not work.
Could someone confirm that this issue was corrected in SimpleLink F3 SDK v9.12, and if not, could you give me an example how to use the workaround in the onoff_switch example?
Thanks,