This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R5: SimpleLink Low Power F3 Demos are now on GitHub!

Part Number: CC2340R5

Tool/software:

Hello everyone,

A GitHub repository hosting SimpleLink F3 SDK examples for CC23XX / CC27XX devices is now available!

https://github.com/TexasInstruments-Sandbox/SimpleLink-Low-Power-F3-Demos 

Featured examples include:

  • UART-based Command Line Interface (CLI) driver
  • BLE UART command line example
  • Brushless DC (BLDC) motor control through UART or BLE
  • Two-digit, 7-segment LCD driver
  • Host for interfacing with the CC2340R5 ROM Serial Bootloader (SBL)
  • Modified PropRF Echo Rx/Tx examples for controlling a stepper motor
  • PWM output wave using DMA transfers
  • Zigbee Window Controller/Covering demos with Brushed DC (BDC) motor control
  • Full BLE GATT Client using GATT API functions to query the GATT table of any central
  • BLE Super Advertiser which broadcasts as much advertisements as possible to stress test centrals

There is also a software tool included: the UniScript CLI HSM Flasher, a Python-based Command-Line Interface (CLI) flasher that supports HSM flashing for the CC27XX family of devices.

For more information, please refer to the GitHub README.

Regards,
Ryan