Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2755R10: Zegbee evalation

Part Number: CC2755R10
Other Parts Discussed in Thread: CC2755P10,

I am reviewing the release notes for the SimpleLink Low Power F3 SDK.

There is no mention of a CC2755R10 LaunchPad, and it states that the CC2745R10 LaunchPad should be used. However, the CC2745 does not support ZigBee. My understanding is that ZigBee evaluation cannot be performed with the CC2745 LaunchPad — is this correct? Also, I see ZigBee sample code for the CC2755P10 LaunchPad in Resource Explorer, but the CC2755P10 LaunchPad does not appear to be available for purchase. Will it be released in the future, and if so, when?

 

Best Regards