Part Number: CC2652P
Other Parts Discussed in Thread: CC1352P, Z-STACK
Hi,
Just saw that the zigbee alliance announced Zigbee 4.0 and Suzi
What is the expected arrival for compatibility of these for cc2652p chipset.
Also, if using the cc1352p chipset, can I use DMM to run these simultaneously ?
From the latest SDK 8.30 (F2 SDK) release notes I can see that the current
Zigbee certified stack - Zigbee Pro 2017 (R22) and Green Power Proxy v1.1.1 (Z-Stack Core v1.0.0.0)
However in the low power F3 SDK (based on ZBOSS ?)
Zigbee certified stack - Zigbee Pro 2023 (R23) and Zigbee Pro 2017 (R22), Green Power Proxy v1.1.2 (Zigbee Core v1.0.0.0)
Is this correct ? please could you share the future roadmap for newer Zigbee Pro versions
Also is the F2 SDK stack also going to be based on ZBOSS in the future ?
Thanks
Akhilesh