Part Number: CC2652RB
Other Parts Discussed in Thread: CC2592, SYSCONFIG, SIMPLELINK-2-4GHZ-DESIGN-REVIEWS
Hello All,
in my project I am using CC2652RB1F and also CC2592. I am using zr_genericapp example. this example is successfully running in TI lancnchpad CC2652RB development kit. but same example is not running in my custom board. i tried to debugging, in main() function code executes still BIOS_start() function, once it reaches this function I am getting below errors.
Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 20.4.0.3756)
Trouble Halting Target CPU: (Error -2064 @ 0x0) Unable to read device status. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 20.4.0.3756)
when I run the normal gpiointrupt examples in custom board it is running. but when I tried with Zstack examples I am geting above errors.
connection between CC2652RB and CC2592 is
DIO20(I removed defult pin assignment MAX25R8035F SPI Flash Chip Select)-->PA_EN,
LNA_EN-->DIO12,
HGM-->DIO4.
FLASH DO-->DIO8
FLASH DI-->DIO9
FLASH CLK--> DIO10
FLASH CS-->DIO11
SWITCH-->DIO13
LED-->DIO6
MEM-RST-->DIO5
RELAY-->DIO15
I am struggling with this issue. any solutions please.
Thank you,