This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2630: SimpleLink SDK sample projects, Z-Stack sample projects

Part Number: CC2630
Other Parts Discussed in Thread: Z-STACK, , CC2650

Currently, we are using a Zigbee module developed with the cc2630F128RHB. However, we haven't found the SimpleLink CC13x0/CC26x0 SDK, and the cc2630 is also not available in Z-Stack Home 1.2.2a. The development board has already been designed, but we can't find any sample projects. We are seeking the corresponding version of the SDK and Z-Stack.

  • Hi a L,

    Z-STACK-ARCHIVE includes Z-STACK-HOME which provides download access to CC2630/CC2650 resources which are typically installed under C:\ti\simplelink\zstack_home_1_02_02a_44539, separate from the CC235X version location.  

    However, I must highly advise against developing Zigbee solutions on the CC2630.  Support for CC26X0 Zigbee has been deprecated for a decade due to the low flash availability on these devices.  TI will give limited to no support on these devices and it is recommended that your project migrate to the SimpleLink F3 SDK and CC2340R5 / CC2755R10 for optimal Zigbee performance and support.

    Regards,
    Ryan