This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R5: Bidirectional Green Power Zigbee Sink

Part Number: CC2340R5
Other Parts Discussed in Thread: SYSCONFIG

Hi Team,

Posting on behalf of our customer.

I am using CC2340r5.I want to develop a receiver with this part which need to accept signals from other grren power zigbee transmitters.I want to send signal if the transmitter is battery supported.I want to confirm if this part number can support my requirement.I started with simple_combo_LP_EM_CC2340R5_freertos_ticlang and gpd_switch.I tried to modify gpd_switch with bidirectional commissioning.BUT failed to make combo with bicommisioning sink.I need help to proceed further

I used the Zigbee Green Power Simple Combo example from GitHub to implement a Green Power Sink, with a gpd_switch as the Green Power Device (GPD). The implementation worked successfully when the switch was configured as unidirectional.

However, when I changed the gpd_switch configuration to bidirectional in SysConfig, the commissioning process started failing.

Could you confirm whether it is possible to implement a bidirectional Green Power Sink using the Simple Combo example?

If so, what additional changes or modifications are required?

Regards,

Danilo