This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652R: RX fails using TI Simplelink SDK 8.30.01.01

Part Number: CC2652R

Hello!

 

We have encountered a problem with our application running as a TI15.4 Coordinator using TI Simplelink SDK 8.30.01.01. 

In the current setup only one channel is configured, which means that no CCA measurements are being made. 

After ~30mins of quite heavy 15.4 traffic to the coordinator the stack stops responding. No callbacks are fired, it does not respond to UHF Scan. In this scenario, if I manually trigger a CCA (energy detect scan through ApiMac_mlmeScanReq) the stack recovers, meaning it responds to UHF scans, callbacks are fired on incoming messages and so on. 

Now, here's the interesting part: If I upgrade the application to TI Simplelink SDK 8.31.00.11 I can no longer reproduce the issue. This brings me to the question:

Is this something you have discovered and fixed in 8.31.00.11?
I can't find anyting in the 8.31.00.11  changelog that matches this behaviour.