This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2430EM Coordinator receive from multiple devices

I'm having trouble wih my Zigbee coordinator receiving from multiple routers. I am running the SerialApp and attempting to send characters over a terminal from 2 PCs with attached RF04EB and CC2430EM boards. I can receive from one but in order to receive then from the other I have to send around 5 or 6 characters before I start to see it on the coordinator's side. Then this process is reversed and I get the same thing. I remember reading somewhere about the sample apps you can't have more than so many devices communicating with a coordinator at one time but is that correct? Is there a define in code or a config file I've overlooked to get the coordinator to receive from multiple devices, specifically routers? Thanks!