Other Parts Discussed in Thread: MSP430F1232, CC2500, MSP430F2012, TEST2
I have a board using CC2500 and MSP430F1232 , sending wireless packets using RF. This board is configured in the TX (TRANSMIT) mode and successfully transmits information every 6 seconds (i am transmitting at zero dbm level- which is almost the highest power level i can transmit information in). There exists another board using CC2500 AND MSP430F1232, waiting to receive packets. I intend to transmit and receive packets in a room with 20m * 20m area. I have followed all the necessary steps required to implement the board in the receive mode, but i do not get any interrupt on receive. The pin 0 on port 0 has been configured to interrupt on the falling edge. Can anyone help me spot the problem? i have used the following settings and my source code is attached.
PORT SETTINGS:-
// --- CC2500 Interface ---
// P1.0 <-- GDO-0 (int)
// P1.1 <-- GDO-2 (int)
// P1.2 --> CSN-CC2500
// P1.3 --> CSEEPROM
// P1.4 --> WPEEPROM
// P1.5 --> UCLK
// P1.6 --> SIMO
// P1.7 --> SOMI
NECESSARY REGISTER SETTINGS:-
IOCFG2 = 0x29 (GDO-2 will be used as default to signal CHPRDY (chip ready))
IOCFG0 = 0x06 (GDO-0 asserted-low when packet received)
PKTLEN = 0x10 (Packet length is 16 bytes)
PKTCTRL1 = 0x00
PKTCTRL0 = 0x84
FREND1 = 0xB6 (Front end RX configuration.)
MCSM1 = 0x00 (return to idle after completing RX)
-------------------------------------------------------------------------------------------------------
SOURCE CODE :-
/*******************************************************************************
*
* File cc2500_TagRx.c
* Description TAGRx implementation for CC2500 & MSP430
*
*
*******************************************************************************///******************************************************************************
// CC2500 TAG-RX Test Code - March 2008
//
//
// MSP430F2012
// ------------
//
// --- CC2500 Interface ---
// P1.0 <-- GDO-0 (int)
// P1.1 <-- GDO-2 (int)
// P1.2 --> CSN-CC2500
// P1.3 --> CSEEPROM
// P1.4 --> WPEEPROM
// P1.5 --> UCLK
// P1.6 --> SIMO
// P1.7 --> SOMI
//
//******************************************************************************
#include "msp430x20x2.h"
//-------------------------------
// CC2500 defines
//-------------------------------
// Configuration Registers
#define TI_CCxxx0_IOCFG2 0x00 // GDO2 output pin configuration
#define TI_CCxxx0_IOCFG1 0x01 // GDO1 output pin configuration
#define TI_CCxxx0_IOCFG0 0x02 // GDO0 output pin configuration
#define TI_CCxxx0_FIFOTHR 0x03 // RX FIFO and TX FIFO thresholds
#define TI_CCxxx0_SYNC1 0x04 // Sync word, high byte
#define TI_CCxxx0_SYNC0 0x05 // Sync word, low byte
#define TI_CCxxx0_PKTLEN 0x06 // Packet length
#define TI_CCxxx0_PKTCTRL1 0x07 // Packet automation control
#define TI_CCxxx0_PKTCTRL0 0x08 // Packet automation control
#define TI_CCxxx0_ADDR 0x09 // Device address
#define TI_CCxxx0_CHANNR 0x0A // Channel number
#define TI_CCxxx0_FSCTRL1 0x0B // Frequency synthesizer control
#define TI_CCxxx0_FSCTRL0 0x0C // Frequency synthesizer control
#define TI_CCxxx0_FREQ2 0x0D // Frequency control word, high byte
#define TI_CCxxx0_FREQ1 0x0E // Frequency control word, middle byte
#define TI_CCxxx0_FREQ0 0x0F // Frequency control word, low byte
#define TI_CCxxx0_MDMCFG4 0x10 // Modem configuration
#define TI_CCxxx0_MDMCFG3 0x11 // Modem configuration
#define TI_CCxxx0_MDMCFG2 0x12 // Modem configuration
#define TI_CCxxx0_MDMCFG1 0x13 // Modem configuration
#define TI_CCxxx0_MDMCFG0 0x14 // Modem configuration
#define TI_CCxxx0_DEVIATN 0x15 // Modem deviation setting
#define TI_CCxxx0_MCSM2 0x16 // Main Radio Cntrl State Machine config
#define TI_CCxxx0_MCSM1 0x17 // Main Radio Cntrl State Machine config
#define TI_CCxxx0_MCSM0 0x18 // Main Radio Cntrl State Machine config
#define TI_CCxxx0_FOCCFG 0x19 // Frequency Offset Compensation config
#define TI_CCxxx0_BSCFG 0x1A // Bit Synchronization configuration
#define TI_CCxxx0_AGCCTRL2 0x1B // AGC control
#define TI_CCxxx0_AGCCTRL1 0x1C // AGC control
#define TI_CCxxx0_AGCCTRL0 0x1D // AGC control
#define TI_CCxxx0_WOREVT1 0x1E // High byte Event 0 timeout
#define TI_CCxxx0_WOREVT0 0x1F // Low byte Event 0 timeout
#define TI_CCxxx0_WORCTRL 0x20 // Wake On Radio control
#define TI_CCxxx0_FREND1 0x21 // Front end RX configuration
#define TI_CCxxx0_FREND0 0x22 // Front end TX configuration
#define TI_CCxxx0_FSCAL3 0x23 // Frequency synthesizer calibration
#define TI_CCxxx0_FSCAL2 0x24 // Frequency synthesizer calibration
#define TI_CCxxx0_FSCAL1 0x25 // Frequency synthesizer calibration
#define TI_CCxxx0_FSCAL0 0x26 // Frequency synthesizer calibration
#define TI_CCxxx0_RCCTRL1 0x27 // RC oscillator configuration
#define TI_CCxxx0_RCCTRL0 0x28 // RC oscillator configuration
#define TI_CCxxx0_FSTEST 0x29 // Frequency synthesizer cal control
#define TI_CCxxx0_PTEST 0x2A // Production test
#define TI_CCxxx0_AGCTEST 0x2B // AGC test
#define TI_CCxxx0_TEST2 0x2C // Various test settings
#define TI_CCxxx0_TEST1 0x2D // Various test settings
#define TI_CCxxx0_TEST0 0x2E // Various test settings
// Strobe commands
#define TI_CCxxx0_SRES 0x30 // Reset chip.
#define TI_CCxxx0_SFSTXON 0x31 // Enable/calibrate freq synthesizer
#define TI_CCxxx0_SXOFF 0x32 // Turn off crystal oscillator.
#define TI_CCxxx0_SCAL 0x33 // Calibrate freq synthesizer & disable
#define TI_CCxxx0_SRX 0x34 // Enable RX.
#define TI_CCxxx0_STX 0x35 // Enable TX.
#define TI_CCxxx0_SIDLE 0x36 // Exit RX / TX
#define TI_CCxxx0_SAFC 0x37 // AFC adjustment of freq synthesizer
#define TI_CCxxx0_SWOR 0x38 // Start automatic RX polling sequence
#define TI_CCxxx0_SPWD 0x39 // Enter pwr down mode when CSn goes hi
#define TI_CCxxx0_SFRX 0x3A // Flush the RX FIFO buffer.
#define TI_CCxxx0_SFTX 0x3B // Flush the TX FIFO buffer.
#define TI_CCxxx0_SWORRST 0x3C // Reset real time clock.
#define TI_CCxxx0_SNOP 0x3D // No operation.
// CC2500 Status registers
#define TI_CCxxx0_PARTNUM 0x30 // Part number
#define TI_CCxxx0_VERSION 0x31 // Current version number
#define TI_CCxxx0_FREQEST 0x32 // Frequency offset estimate
#define TI_CCxxx0_LQI 0x33 // Demodulator estimate for link quality
#define TI_CCxxx0_RSSI 0x34 // Received signal strength indication
#define TI_CCxxx0_MARCSTATE 0x35 // Control state machine state
#define TI_CCxxx0_WORTIME1 0x36 // High byte of WOR timer
#define TI_CCxxx0_WORTIME0 0x37 // Low byte of WOR timer
#define TI_CCxxx0_PKTSTATUS 0x38 // Current GDOx status and packet status
#define TI_CCxxx0_VCO_VC_DAC 0x39 // Current setting from PLL cal module
#define TI_CCxxx0_TXBYTES 0x3A // Underflow and # of bytes in TXFIFO
#define TI_CCxxx0_RXBYTES 0x3B // Overflow and # of bytes in RXFIFO
#define TI_CCxxx0_NUM_RXBYTES 0x7F // Mask "# of bytes" field in _RXBYTES
// CC2500 Other memory locations
#define TI_CCxxx0_PATABLE 0x3E
#define TI_CCxxx0_TXFIFO 0x3F
#define TI_CCxxx0_RXFIFO 0x3F
// CC2500 Masks for appended status bytes
#define TI_CCxxx0_LQI_RX 0x01 // Position of LQI byte
#define TI_CCxxx0_CRC_OK 0x80 // Mask "CRC_OK" bit within LQI byte
// CC2500 Definitions to support burst/single access:
#define TI_CCxxx0_WRITE_BURST 0x40
#define TI_CCxxx0_READ_SINGLE 0x80
#define TI_CCxxx0_READ_BURST 0xC0
//-------------------------------
// 25LC256 EEPROM defines
//-------------------------------
#define EEPROM_WREN 0x06 // EEPROM Write Enable Instruction
#define EEPROM_WRITE 0x02 // EEPROM Write Instruction
#define EEPROM_READ 0x03 // EEPROM Read Instruction
#define EEPROM_RSR 0x05 // EEPROM Read Status Register Instruction
//-------------------------------
// General defines
//-------------------------------
#define TRUE 1
#define FALSE 0
#define PAYLOAD_SIZE 16
#define CHANNEL_1 20 // RF Channel for TAG Scan
#define CHANNEL_2 21 // RF Channel for TAG Read-Write transaction
#define TEMPERATURE 0x00
#define BATTERY 0x01
#define ZERODBM 0xFE // 0dBm is default Tx Power
#define TAG_UID_SET 0x3C // UID Set Command
#define TAG_BASIC 0x10
#define TAG_SENSO 0x20
#define TAG_LOGGO 0x30
#define TI_CC_SPI_USART0_PxIN P1IN // MSP430 SPI Port
#define TI_CC_SPI_USART0_SOMI 0x80 // for MSP430F2012 SOMI is P1.7
//-------------------------------
// Global variables
//-------------------------------
unsigned char tx_array [20], rx_array [20]; // tx and rx data arrays
unsigned char uid [5] = {0xAA,0xBB,0xCC,0xDD,0xEE}; // UID array-default UID, Rx-Address is UID first 5 bytes
char tx_finished, rx_finished; // RF interface status variables
char payload_sentreceived = FALSE; // RF interface status variables
char stat_CC2500;
signed char tx_count, rx_count; // index counters
unsigned int i,j; // index counters
unsigned int wait_count; // random wait count
int battery_voltage; // battery voltage value after ADC
unsigned int wakeup_tick = 1; // wakeup counter
unsigned char sr1,sr2,sr3,sr4; // shift register values for randomizer
char timeout;
char CC2500_error;
unsigned char rssi;
unsigned int test_count = 0;
unsigned char dummy;
//-------------------------------
// Function Declarations
//-------------------------------
void randomizer (void);
void txmit_id (void);
void write_uid (void);
void read_uid(void);
void powerdown_rf (void);
void por_CC2500 (void);
void write_CC2500_reg (char reg, char data);
void write_CC2500_commandstrobe (char command_strobe);
void burstwr_CC2500_FIFO (void);
void txmit_payload (char channel);
unsigned char read_CC2500_statusreg (unsigned char reg);
void rcv_payload (void);
void init_CC2500_default (void);
void init_CC2500_rx (char channel);
int read_adc (char temp_or_bat);
void main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
BCSCTL3 = XCAP_2; // 10pF cap selected to provide 10+2//10+2 = 6pF as load cap
for (j=0; j<10000; j++); // Delay for DCO to stabilize
BCSCTL1 = CALBC1_8MHZ; // DCO=8MHz, ACLK=32768Hz
DCOCTL = CALDCO_8MHZ;
FCTL2 = FWKEY + FSSEL0 + FN4 + FN3; // MCLK/(24+1) for Flash Timing Generator
// Init Digital I/O ports
P1OUT = 0x1C; // Set CS2500, CSEEPROM, WREEPROM high
P1DIR = 0x1C; // Set P1.2, P1.3, P1.4 output
P1IE |= 0x01; // P1.0 interrupt enabled
P1IES |= 0x01; // P1.0 = CC2500 GDO-0, Hi-to-low edge asserted when packet received
P1IFG &= ~0x01; // P1.0 IFG cleared
// Init Timer-A0 for LPM3 wakeup
// TACTL = TASSEL_1 + ID_1 + MC_1; // TACLK = ACLK, /2 clk-divide, Up mode to CCR0.
// TACCR0 = 32768; // Settings for Period = 1 sec
// TACCTL0 |= CCIE; // Compare-mode interrupt enabled.
// Init USI Module to SPI Mode
USICTL0 |= USISWRST; // Hold SPI in Reset state
USICTL0 = USIPE7 + USIPE6 + USIPE5 + USIMST + USIOE; // Enable SDI,SDO,SCLK, SPI Master Mode, USI output enable
USICTL1 = USICKPH + USIIE; // Clock phase select, USI counter interrupt enable
USICKCTL = USISSEL1; // SPICLK = SMCLK
USISRL = 0x00; // Ensure SDO low instead of high
USICTL0 &= ~USISWRST; // Enable SPI operation
_EINT();
por_CC2500 ();
init_CC2500_default();
dummy = read_CC2500_statusreg (TI_CCxxx0_PARTNUM);
dummy = read_CC2500_statusreg (TI_CCxxx0_RXBYTES);
write_CC2500_commandstrobe(TI_CCxxx0_SFRX); // Flush RX buffer
while (1)
{
payload_sentreceived = FALSE;
init_CC2500_rx (CHANNEL_1);
do
{
LPM0;
}
while (!payload_sentreceived);
rcv_payload ();
++test_count;
} /*------------End of endless while----------*/
} /*------------End Main----------*/
//-----------------------------------------------------------------------------
// TAG and Reader interface packet handling routines
//-----------------------------------------------------------------------------
void randomizer ()
{
unsigned char e1,e2,e3,e4,fb,t;
for (j=0; j<8; j++) // turn 8 times for byte value
{
e1 = sr1 >> 6; // bit-2
e2 = sr1 >> 7; // bit-1
e3 = sr3 >> 2; // bit-22
e4 = sr4 & 0x01; // bit-32
fb = e1 ^ e2 ^ e3 ^ e4; // XOR all bits
sr4 = (sr4 >> 1); // shift all sr values right
t = sr3 << 7;
sr4 |= t;
sr3 = (sr3 >> 1);
t = sr2 << 7;
sr3 |= t;
sr2 = (sr2 >> 1);
t = sr1 << 7;
sr2 |= t;
sr1 = (sr1 >> 1);
sr1 |= (fb << 7); // feed the fb value to 1st bit
}
}
void txmit_id (void)
{
for (j=0; j<5; j++) tx_array [j] = uid [4-j];
for (j=0; j<8; j++) tx_array [j+5] = 0xA3; // dummy data
tx_array [13] = (char) battery_voltage; // battery voltage-LSB
tx_array [14] = (char) (battery_voltage >> 8); // battery voltage-MSB
tx_array [15] = TAG_BASIC; // First byte describes the TAG type
txmit_payload (CHANNEL_1); // txmit SID packet
}
void write_uid ()
{
char *Flash_ptrC; // Segment C pointer
Flash_ptrC = (char *) 0x1040; // Initialize Flash segment C pointer
FCTL1 = FWKEY + ERASE; // Set Erase bit
FCTL3 = FWKEY; // Clear Lock bit
*Flash_ptrC = 0; // Dummy write to erase Seg-C
for (j=0; j<30000; j++);
FCTL1 = FWKEY + WRT; // Set WRT bit for write operation
*Flash_ptrC++ = 0x55; // Segment in use mark
for (j=0; j<5; j++) *Flash_ptrC++ = rx_array [13-j]; // Write UID to Seg-C
FCTL1 = FWKEY; // Clear WRT bit
FCTL3 = FWKEY + LOCK; // Set LOCK bit
read_uid();
}
void read_uid(void) // Reads UID from Seg-C or Seg-D
{ // 1st byte = 0x55 if valid UID is present in the Segment
char *Flash_ptrC; // Segment C pointer
Flash_ptrC = (char *) 0x1040; // Initialize Flash segment C pointer
if (*Flash_ptrC++ == 0x55) for (j=0; j<5; j++) uid [j] = *Flash_ptrC++;
sr1 = uid [1];
sr2 = uid [2];
sr3 = uid [3];
sr4 = uid [4];
}
//-----------------------------------------------------
// CC2500 interface routines
//-----------------------------------------------------
void powerdown_rf (void)
{
write_CC2500_commandstrobe (TI_CCxxx0_SPWD); // powerdown CC2500
}
void por_CC2500 (void)
{
P1OUT |= 0x04; // Set CS-CC2500 High
for (j=0; j<100; j++); // ~40us delay
P1OUT &= ~0x04; // Set CS-CC2500 Low
for (j=0; j<100; j++); // ~40us delay
P1OUT |= 0x04; // Set CS-CC2500 High
for (j=0; j<150; j++); // ~70us delay
P1OUT &= ~0x04; // Set CS-CC2500 Low
while (TI_CC_SPI_USART0_PxIN & TI_CC_SPI_USART0_SOMI); // Wait for CC2500 ready
tx_finished = 0;
rx_count = 0;
tx_count = 0;
USISRL = TI_CCxxx0_SRES; // Write commandstrobe
USICNT = 0x08; // Write the no of bits (8) to be txmitted
do // SPI Tx Started
{
LPM0;
}
while (!tx_finished);
while (TI_CC_SPI_USART0_PxIN & TI_CC_SPI_USART0_SOMI); // Wait for CC2500 ready
P1OUT |= 0x04; // Set CS-CC2500 High
}
void write_CC2500_reg (char reg, char data)
// Writes the data to CC2500 register
{
tx_finished = 0;
rx_count = 0;
tx_count = 1;
tx_array [0] = data;
P1OUT &= ~0x04; // Set CS2500 Low to start SPI cycle
while (TI_CC_SPI_USART0_PxIN & TI_CC_SPI_USART0_SOMI); // Wait for CC2500 ready
USISRL = reg; // register-wr, no-burst
USICNT = 0x08; // Write the no of bits (8) to be txmitted
do // SPI Tx Started
{
LPM0;
}
while (!tx_finished);
P1OUT |= 0x04; // Set CS2500 High to finish SPI cycle
stat_CC2500 = rx_array [0]; // CC2500 status is read after first byte wr
}
void write_CC2500_commandstrobe (char command_strobe)
// Writes the command strobe to CC2500
{
tx_finished = 0;
rx_count = 0;
tx_count = 0;
P1OUT &= ~0x04; // Set CS2500 Low to start SPI cycle
while (TI_CC_SPI_USART0_PxIN & TI_CC_SPI_USART0_SOMI); // Wait for CC2500 ready
USISRL = command_strobe; // Write commandstrobe
USICNT = 0x08; // Write the no of bits (8) to be txmitted
do // SPI Tx Started
{
LPM0;
}
while (!tx_finished);
P1OUT |= 0x04; // Set CS2500 High to finish SPI cycle
stat_CC2500 = rx_array [0]; // CC2500 status is read after commandstrobe wr
}
unsigned char read_CC2500_statusreg (unsigned char reg)
// Reads the data from CC2500 register
{
tx_finished = 0;
rx_count = 0;
tx_count = 1;
tx_array [0] = 0x55; // dummy data
P1OUT &= ~0x04; // Set CS2500 Low to start SPI cycle
while (TI_CC_SPI_USART0_PxIN & TI_CC_SPI_USART0_SOMI); // Wait for CC2500 ready
USISRL = (reg | TI_CCxxx0_READ_BURST); // register-rd, no-burst
USICNT = 0x08; // Write the no of bits (8) to be txmitted
do // SPI Tx Started
{
LPM0;
}
while (!tx_finished);
P1OUT |= 0x04; // Set CS2500 High to finish SPI cycle
stat_CC2500 = rx_array [0];
return (rx_array[1]); // CC2500 status-reg is read as second byte
}
void burstwr_CC2500_FIFO (void)
// writes PAYLOAD_SIZE byte tx-data to TX FIFO
// assumes data is preloaded in tx_array
// PAYLOAD_SIZE must be > 1
{
tx_finished = 0;
rx_count = 0;
tx_count = PAYLOAD_SIZE;
P1OUT &= ~0x04; // Set CS2500 Low to start SPI cycle
while (TI_CC_SPI_USART0_PxIN & TI_CC_SPI_USART0_SOMI); // Wait for CC2500 ready
USISRL = (TI_CCxxx0_TXFIFO | TI_CCxxx0_WRITE_BURST); // TX-FIFO-wr, burst-mode
USICNT = 0x08; // Write the no of bits (8) to be txmitted
do // SPI Tx Started
{
LPM0;
}
while (!tx_finished);
P1OUT |= 0x04; // Set CS2500 High to finish SPI cycle
stat_CC2500 = rx_array [0]; // CC2500 status is read after first byte wr
}
void txmit_payload (char channel)
{
// while (read_CC2500_statusreg (TI_CCxxx0_TXBYTES) < PAYLOAD_SIZE); // wait for TX FIFO empty
// write_CC2500_reg (TI_CCxxx0_CHANNR, channel); // set Channel number
burstwr_CC2500_FIFO (); // fill the TX FIFO
write_CC2500_commandstrobe (TI_CCxxx0_STX); // start TX
// powerdown_rf ();
}
void rcv_payload (void)
// wait for RX, read CC2500 PAYLOAD,
// returns in rx_array
// read RSSI
{
unsigned char no_bytes_rcvd;
for (j=0; j<1500; j++);
CC2500_error = FALSE;
// write_CC2500_commandstrobe(TI_CCxxx0_SFRX); // Flush RX buffer
no_bytes_rcvd = read_CC2500_statusreg (TI_CCxxx0_RXBYTES);// read no of bytes rcvd
// no_bytes_rcvd = 0x10;
// if (no_bytes_rcvd > PAYLOAD_SIZE)
// {
// write_CC2500_commandstrobe(TI_CCxxx0_SFRX); // more bytes are read than expected, flush RX Buffer
// CC2500_error = TRUE;
// }
// else
// {
tx_finished = FALSE;
rx_count = 0;
tx_count = no_bytes_rcvd;
for (j=0; j<no_bytes_rcvd; j++) tx_array [j] = 0x55; // dummy data
P1OUT &= ~0x04; // Set CS2500 Low to start SPI cycle
while (TI_CC_SPI_USART0_PxIN & TI_CC_SPI_USART0_SOMI); // Wait for CC2500 ready
USISRL = (TI_CCxxx0_RXFIFO | TI_CCxxx0_READ_BURST); // RX-FIFO-rd, burst-mode // register-rd, no-burst
USICNT = 0x08; // Write the no of bits (8) to be txmitted
do // SPI Tx Started
{
LPM0;
}
while (!tx_finished);
P1OUT |= 0x04; // Set CS2500 High to finish SPI cycle
stat_CC2500 = rx_array [0]; // CC2500 status-reg is read as second byte
rssi = read_CC2500_statusreg (TI_CCxxx0_RSSI); // read RSSI value
// }
}
void init_CC2500_rx (char channel)
{
// write_CC2500_reg (TI_CCxxx0_CHANNR, channel); // set Channel number
write_CC2500_commandstrobe (TI_CCxxx0_SRX); // Start RX
}
void init_CC2500_default (void)
// Product = CC2500
// Crystal accuracy = 40 ppm
// X-tal frequency = 26 MHz
// RF output power = 0 dBm
// RX filterbandwidth = 540.000000 kHz
// Deviation = 0.000000
// Return state: Return to RX state upon leaving either TX or RX
// Datarate = 250.000000 kbps
// Modulation = (7) MSK
// Manchester enable = (0) Manchester disabled
// RF Frequency = 2433.000000 MHz
// Channel spacing = 199.950000 kHz
// Channel number = 0
// Optimization = Sensitivity
// Sync mode = (3) 30/32 sync word bits detected
// Format of RX/TX data = (0) Normal mode, use FIFOs for RX and TX
// CRC operation = (1) CRC calculation in TX and CRC check in RX enabled
// Forward Error Correction = (0) FEC disabled
// Length configuration = (1) Fixed length packets
// Packetlength = 16
// Preamble count = (2) 4 bytes
// Append status = 1
// Address check = (0) No address check
// FIFO autoflush = 0
// Device address = 0
// GDO0 signal selection = (0X47) Asserts when packet received, and de-asserts when first byte is read from FIFO
// GDO2 signal selection = (0X29) CHPRDY
{
// Write register settings
write_CC2500_reg (TI_CCxxx0_IOCFG2, 0x29); // GDO-2 will be used as default to signal CHPRDY (chip ready)
write_CC2500_reg (TI_CCxxx0_IOCFG0, 0x06); // GDO-0 asserted-low when packet received
write_CC2500_reg (TI_CCxxx0_PKTLEN, 0x10); // Packet length is 16 bytes
write_CC2500_reg (TI_CCxxx0_PKTCTRL1, 0x00); // Packet automation control.
write_CC2500_reg (TI_CCxxx0_PKTCTRL0, 0x84); // Packet automation control.
write_CC2500_reg (TI_CCxxx0_ADDR, 0x01); // Device address.
write_CC2500_reg (TI_CCxxx0_CHANNR, 0x05); // Channel number.
write_CC2500_reg (TI_CCxxx0_FSCTRL1, 0x07); // Freq synthesizer control.
write_CC2500_reg (TI_CCxxx0_FSCTRL0, 0x00); // Freq synthesizer control.
write_CC2500_reg (TI_CCxxx0_FREQ2, 0x5D); // Freq control word, high byte
write_CC2500_reg (TI_CCxxx0_FREQ1, 0x93); // Freq control word, mid byte.
write_CC2500_reg (TI_CCxxx0_FREQ0, 0xB1); // Freq control word, low byte.
write_CC2500_reg (TI_CCxxx0_MDMCFG4, 0x2D); // Modem configuration.
write_CC2500_reg (TI_CCxxx0_MDMCFG3, 0x3B); // Modem configuration.
write_CC2500_reg (TI_CCxxx0_MDMCFG2, 0x73); // Modem configuration.
write_CC2500_reg (TI_CCxxx0_MDMCFG1, 0x22); // Modem configuration.
write_CC2500_reg (TI_CCxxx0_MDMCFG0, 0xF8); // Modem configuration.
write_CC2500_reg (TI_CCxxx0_DEVIATN, 0x00); // Modem dev (when FSK mod en)
write_CC2500_reg (TI_CCxxx0_MCSM1 , 0x00); // MainRadio Cntrl State Machine
write_CC2500_reg (TI_CCxxx0_MCSM0 , 0x18); // MainRadio Cntrl State Machine
write_CC2500_reg (TI_CCxxx0_FOCCFG, 0x1D); // Freq Offset Compens. Config
write_CC2500_reg (TI_CCxxx0_BSCFG, 0x1C); // Bit synchronization config.
write_CC2500_reg (TI_CCxxx0_AGCCTRL2, 0xC7); // AGC control.
write_CC2500_reg (TI_CCxxx0_AGCCTRL1, 0x00); // AGC control.
write_CC2500_reg (TI_CCxxx0_AGCCTRL0, 0xB2); // AGC control.
write_CC2500_reg (TI_CCxxx0_FREND1, 0xB6); // Front end RX configuration.
write_CC2500_reg (TI_CCxxx0_FREND0, 0x10); // Front end TX configuration.
write_CC2500_reg (TI_CCxxx0_FSCAL3, 0xEA); // Frequency synthesizer cal.
write_CC2500_reg (TI_CCxxx0_FSCAL2, 0x0A); // Frequency synthesizer cal.
write_CC2500_reg (TI_CCxxx0_FSCAL1, 0x00); // Frequency synthesizer cal.
write_CC2500_reg (TI_CCxxx0_FSCAL0, 0x11); // Frequency synthesizer cal.
write_CC2500_reg (TI_CCxxx0_FSTEST, 0x59); // Frequency synthesizer cal.
write_CC2500_reg (TI_CCxxx0_TEST2, 0x88); // Various test settings.
write_CC2500_reg (TI_CCxxx0_TEST1, 0x31); // Various test settings.
write_CC2500_reg (TI_CCxxx0_TEST0, 0x0B); // Various test settings.
write_CC2500_reg (TI_CCxxx0_PATABLE, ZERODBM); // Set TX Power Level to 0 dBm
// always txmit at max power level (0dBm)
}
//-----------------------------------------------------------------------------
// A/D Converter Interface Routines
//-----------------------------------------------------------------------------
int read_adc (char temp_or_bat)
{
int conversion;
if (temp_or_bat == TEMPERATURE) ADC10CTL1 = ADC10DIV_3 + INCH_10 + SHS_0 + CONSEQ_0;
else ADC10CTL1 = ADC10DIV_3 + INCH_11 + SHS_0 + CONSEQ_0;
ADC10CTL0 = SREF_1 + ADC10SHT_3 + ADC10SR + REFON + ADC10ON;
// VR+=VREF+ and VR-=VSS, 64xADC10CLKs SH time
// Sample Rate=50ksps, Ref is on and=1.5V
for (j=1; j<80; j++); // > 30uS delay to settle VRef
ADC10CTL0 |= ENC + ADC10SC; // ADC10 Enable conversion and start conversion
while (!(ADC10IFG & ADC10CTL0)); // Wait for conversion to finish
conversion = ADC10MEM;
ADC10CTL0 &= ~(ADC10IFG + ENC); // Clear ENC and IFlag
ADC10CTL0 &= ~(ADC10ON + REFON); // Shutdown ADC
return (conversion);
}
//-----------------------------------------------------------------------------
// Interrupt Service Routines
//-----------------------------------------------------------------------------
#pragma vector=USI_VECTOR
__interrupt void USI_txrx (void)
{
_BIC_SR_IRQ(LPM0_bits); // Clear LPM0 bits from 0(SR)
tx_count--;
if (tx_count < 0)
{
USICTL1 &= ~0x01; // Clear USIIFG
tx_finished = 0x01;
rx_array [rx_count] = USISRL;
++rx_count;
}
else
{
rx_array [rx_count] = USISRL;
USISRL = tx_array [tx_count];
USICNT = 0x08; // Write the no of bits (8) to be txmitted
++rx_count;
}
}
// Port 1 interrupt service routine for CC2500 INT
#pragma vector=PORT1_VECTOR
__interrupt void Port_1(void)
{
_BIC_SR_IRQ(LPM0_bits); // Clear LPM0 bits from 0(SR)
P1IFG &= ~0x01; // P1.0 IFG cleared
payload_sentreceived = TRUE; // CC2500 GDO-0 INT meaning RX event occured
}
#pragma vector=TIMERA0_VECTOR
__interrupt void ta0_isr(void)
{
LPM3_EXIT; // Exit LPM3 on return
timeout = TRUE;
}