Other Parts Discussed in Thread: Z-STACK, CC2430
I like to understand about the 'Role of Coordinator' much more with respect to Zigbee. Like to clarify the following when a Coordinator power down and powers up during a network is active.
- Coordinator is the one which forms the network and network can exists even if coordinator goes down, is it right? if right, is there any advantage or disadvantage?
- Can a coordinator join to the same network after power down and power up. example., consider a coordinator is powered on with a fixed channel(say 3) and fixed PAN ID (say 20), thereby forming a network with routers and end device on the same channel 3 and PAN ID 20. Can the coordinator will be able to join the same channel 3 and PAN ID 20 when it is power down and powered up again?
- With ZASA application, coordinator joins the network when there is ONLY end devices connected to it. i.e., the coordinator is powered up and forms a network with only end devices (star network), Coordinator is now powered down and powered up, the coordinator joins to the existing network with already defined channel and PAN ID. But it doesn't able to join the network when there is router and end device connected (mesh network). why so?
- Is there any other specific characteristics of Coordinator?