Hi!
1. Question
I'm builing a Network consists of a Coordinator and an End Device. For that I used the SE Sample Application without Security an the transmission function well. So now I want to change the APS Payload cause I'm trying to send an 50 Byte Data Frame from the End Device to the Coordinator. But I don't know if it's possibile to change this and where.
2. Question
I'm trying to build a Network where the End Device sleeps the most time. Can someone explain me how often I have to send the Data from the End Device to the Coordinator. Or what other transmissions are needed for this Network? I've enabled the POWER_SAVING compile option and set in the f8wconfig.cfg the POLL_RATE=0 for the End Device but I still have every 100ms peaks. Where does this peaks come from and where in the SE Sample App can I change this?
I hope someone can help me and that my questions are not to supid.