Other Parts Discussed in Thread: Z-STACK, CC2430, CC2431, FLASH-PROGRAMMER
Hello
I have problem withthe Location Engine example, I can't connect to the Dongle.
I have build as in the example in Z-Stack User's Guide - CC2431DB (F8W-2006-0025).pdf
One CC2430 at EB as Coordinator LOCATION_DONGLE
One CC2431 at BB as Router LOCATION_BLINDNODE
One CC2431 at BB as Router LOCATION_REFNODE
I have the RF04EB connected to the computer with both the USB and the serial cable but when I start the Z-Location Engine CC2431 it says “Dongle: Disconnected” and nothing happens.
I have also tried to run the precompiled hex files but with no luck.
What can be wrong and what should I do?
I have:
1 piece RF04EB 1.9
2 piece SOC BB 1.1
2 piece CC2431DK_EM_Blind Rev 1.3
1 piece CC2430DK_EM Rev 1.6
ZStack-1.4.3-1.2.1
Regards Tobias