This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

max number of message clusters

hello

Is there a maximum number of message clusters ?

  • I can't dig into the code to find out the exact number, but it's likely a 16-bit number or 65536. Home Automation uses about 70 clusters. Do you have an application that requires a lot more than this?

    Scott

  • thanks

    I have add 10 clusters to the existing 9 in location code, and I encountered several conflicts , outgoing clusters cause wrong incoming cluster, not  expected

    but maybe it come  from my interface and serial I/O , and not zstack if you say 70 clusters is possible